I am designing a circuit with input being supplied by a 3.7 V (nominal) Li-Ion battery and the output is fixed 3.3 V. Majority of time, the input voltage will be greater than 3.3 V but as the battery drains the input voltage may drop to 3 V. There is also a battery switch that can disconnect the battery from the circuit. Under these conditions, is it possible to eliminate RC circuit between Vin and VINA and have VINA pin directly connected to Vin pin?
I will appreciate clarification on the reason for the RC filter. It appears that with this RC circuit in place, when the battery is switched on the voltage on VINA pin will rise slowly, but when switching off VINA pin will have the full battery voltage, where as Vin pin will have 0 voltage, which will rise slowly by capacitor through the resistor (of RC circuit) and eventually dropping back to zero, as capacitor discharges.
Kind Regards,
Sudhir Gupta