Dear TI-Team,
I wonder what the maximum output voltage of the LMR36506 in the adjustable version is. I cannot find any hint in the datasheet that it is limited to less than the dropout voltage due to the maximum ontime limitation but WEBENCH omits this part when I choose an output voltage of more than 24V.
For my application I've got an input voltage of 48V nom. and want to generate an output voltage of approx 40V. When operating at 400kHz that should IMHO not mess with neither maximum ontime nor with minimum offtime, so where does the 24V limitation come from?
Best regards
Robin