Part Number: LM2759
In LM2759 datasheet i have some doubt regarding the given information,
FLASH TIME-OUT FEATURE
Time-out Protection Circuitry disables the current sink when either the Strobe pin is held at logic high or the
Flash mode is enabled via the I2C compatible interface longer than the programmed timeout duration. This
prevents the device from self-heating due to the high power dissipation during Flash conditions. During the timeout
condition, voltage will still be present on VOUT but the current sink will be shut off, resulting in no current
through the Flash LED. When the device goes into a time-out condition, disabling and then re-enabling the
device will reset the time-out. Use the table below to set the desired Flash timeout duration.
the above passage is in datasheet, in that it is given that "disabling and then re-enabling the
device will reset the time-out", does it mean disabling and re-enabling the strobe pin or the entire device ??