Other Parts Discussed in Thread: BQSTUDIO, BQ25790,
Is the BQ25790EVM with the File "3618.Charger_2_00-bq25790_92.bqz" compatible with the BQStudio v1.3.101? If I select the downloaded file of the BQ25790 there is the following message shown to me:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the BQ25790EVM with the File "3618.Charger_2_00-bq25790_92.bqz" compatible with the BQStudio v1.3.101? If I select the downloaded file of the BQ25790 there is the following message shown to me:
Hi Mopa,
The BQZ file for 790/92 was tested in the stable version of BQStudio, 1.3.86. I just download 1.3.101 BQSTUDIO test version and the BQZ file for 790/92 opened without error. Is the BQZ corrupted? I have attached the BQZ file. If you still have errors, I suggest downloading BQSTUDIO 1.3.86.
Regards,
Hi Jeff,
Thanks for the quick response. I have tested the BQZ-File with both BQStudio Versions 1.3.86 and 1.3.101 without success. A complete uninstall and reinstall did also not help and the "Process?-Message" still appears.
Are there other dependencies of the application? I did also start the BQStudio in compatibility Mode.
Regards,
Patrick