Part Number: TPS54418
Other Parts Discussed in Thread: LMQ61460-Q1, SN74HC367
Hi,
I am testing TPS54418EVM to achieve external SYNC functionality with the following specs:
Vin = 3.3V, Vout = 0.85V, Iout = 1.6A
Fsync = 500kHz to 2MHz
While synchronizing to external frequency, the output of the device goes unstable. Please find the attached slide deck with observations. Can someone please look at it and retest on the EVM? Or share any thoughts why such behaviour is observed?
Thank you.TPS54418-Sync-Issue.pptx
Regards,
Sanjay R. Pithadia