Other Parts Discussed in Thread: TPSM53602
Hello all,
I am in the design process right now and I am curious: Could I drive two PTN78020's with a single power supply and get decent results? Say I have one set up to output 3.3V and the other set up for 5V. If I drive both with a 20V @ 2.5A signal, could expect to get ~1.25A output from both? Is there anything I could do to assure that something close to that would happen? Or would I have to use a separate power supply to drive each PTN78020W?
Thank you,
Cole