Part Number: LM5118
Using the 5118 EVAL board and design aid, I tried to get the layout of my board as close as I could to the eval board and the components spec'd according to what was called out in the design aid (admittedly using a 10uH inductor with similar current specs instead of the 7uH that was suggested for my application).
The goal of this application was to have the board act as a 5-16VIn, 12Vout regulator to keep some auxiliary electronics alive during fluctuations during engine start, but also keep said electronics live during key off, but 'disconnect' its loads on the output when the battery voltage dropped to ~12.0-12.1V while in a 'key off' state. Ideally to not let this circuit drain the battery. If a disconnect event happened, the ignition input would override the turn off. The spec sheet says that the board enters a shutdown state at <0.5V on the enable pin. I'm only getting about 10mV on the output side. The board is drawing 30mA when ignition power is applied (guessing that's just the dividers bleeding)..
As of now:
- Voltage in the middle of RDIV1 and RDIV2 is 0.547V with 12.8V present at VIN(CN-1) and no ignition override. Confirmed this is getting to the VIN pin on the 5118.
- Voltage in the middle of RDIV1 and RDIV2 is 4.1V with 12.8V present at VIN(CN-1) and IGNITION IN(CN1-3) brought to 12.8V. Confirmed this is getting to the VIN pin on the 5118.
Attached schematic, png of board, and gerber file. Could you give me some pointers on where I should start troubleshooting?Gerber_TM LVD PCB (1).zipSchematic_TM LVD_2020-08-20_14-11-13.pdfPCB_TM LVD PCB_2020-08-20_14-09-51.pdf