This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63802EVM: TPS63802EVM: Efficiency problems.

Part Number: TPS63802EVM
Other Parts Discussed in Thread: TPS63802

Hi,

I am using the TPS63802 in a low power design.  I tested the TPS63802 with a power supply for Vin and a constant current load of 5mA.

My measured values are:

Vin Cin (mA) Vout Cout* (mA) Eff (%)
4.2 4.82 3.329 5 0.822219
3.7 5.7 3.353 5 0.794927
3.2 6.47 3.337 5 0.805883
3 6.95 3.332 5 0.799041
2.5 8.39 3.337 5 0.795471
2 10.64 3.322 5 0.780545

Is there something I need to changed to get the higher efficiency numbers?  I was expecting numbers in the 90%.  

Thanks