Other Parts Discussed in Thread: TPS63802
Hi,
I am using the TPS63802 in a low power design. I tested the TPS63802 with a power supply for Vin and a constant current load of 5mA.
My measured values are:
Vin | Cin (mA) | Vout | Cout* (mA) | Eff (%) |
4.2 | 4.82 | 3.329 | 5 | 0.822219 |
3.7 | 5.7 | 3.353 | 5 | 0.794927 |
3.2 | 6.47 | 3.337 | 5 | 0.805883 |
3 | 6.95 | 3.332 | 5 | 0.799041 |
2.5 | 8.39 | 3.337 | 5 | 0.795471 |
2 | 10.64 | 3.322 | 5 | 0.780545 |
Is there something I need to changed to get the higher efficiency numbers? I was expecting numbers in the 90%.
Thanks