This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: TPS61169

Part Number: TPS61169
Other Parts Discussed in Thread: TPS61170

Hi,

I am designing a IR LED driver using TPS61169.

The design requirements are follows:

Vin(max)= 5V

Vout(max)= 13V

Iout(max)= 100mA

As per my calculation I selected 10uH inductor. for the this design. Also in we bench i simulated this design for TPS61170. But the TPS61170 has external compensation . So i select TPS61169. So can I follow the same simulation result of TPS61170 for TPS61169?