Hi Ti:
On the datasheet of TPS748, it features the the output CAP >= 2.2uf. Does that mean the any output CAP more than 2.2uF is Ok for stability? 100uF, 200uF, 500uF...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti:
On the datasheet of TPS748, it features the the output CAP >= 2.2uf. Does that mean the any output CAP more than 2.2uF is Ok for stability? 100uF, 200uF, 500uF...
OK. Thank you for sharing. We also have the TPS7A83A which is also a very fast load transient LDO. The advantage this has over the TPS748 is that it has our Any_out feature which allows you to set VOUT without external resistors. This means that the output accuracy is much better as you do not need to consider the accuracy of the feedback resistors.