This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: Copper foil thickness of PCB

Part Number: TPS63070

Hi Team,

Would you advise below 3 questions about heat radiation design?

Regarding TPS63070 datasheet(Section 11.2 Layout Example) or

TPS630702EVM(Section 3.1 TPS630702EVM Layout).

1.I think that the measurement of the junction temperature is based on the standard test specified by JEDEC.

   Is the layout proposed in the data sheet assuming a copper foil thickness of 70um?

2.What is the via size under the choke coil L1, L1 (9 Pin) and L2 (11 Pin) terminals of TPS63070 in the

   layout example? Also, is the via below the L1/L2 terminals filled with holes?

3.What are the copper foil thickness (12um/18um/35um/70um) and the number of layers

   (2 layers/4 layers) of the evaluation board? Also, is there any information such as the

   recommended copper foil thickness or the copper foil thickness assumed in design?

Thanks

Best regards,

Shidara