This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2980: WHen Charger is connected Charging is not done

Part Number: BQ2980
Other Parts Discussed in Thread: BQ24600

I have designed Li-ion battery Protection using BQ2980. I have used reference schematic of BQ2980.

During Normal DSG FET and CHG FET both are ON but when I connect Charger, charging is n't started. I am using 3A charger built using Bq24600 for 1S6P Li-ion Cell.

What will be the possible cause for this? What is voltage difference is required between Battery Voltage and Charger voltage so that Charging is started?

Is there any limitation of charging Current?

When I bypass Protection circuit charge circuit works perfectly.

Regards,

Virendra