Hi Team,
We are using LP8556 LED driver. it seems that has noise issue.
1. we are looking for pure current controlled (Analog based ) LED driver
2. it should be non-switching regulator type LED driver to suppress switching noise.
3. input is 5V. we don't need more than 5V supply for LEDs. PWM is input.
4. we can controll each channels of LED driver by programming.
5. required minimum 3/4 channels and maximum LEDs in a channel is 3
6. LEDs should glow off, when we give Zero duty cycle of PWM.
7. Maximum current per channel should be at 100mA.
8. it is used in medical endoscopy. so LED driver should have camera application. not back light LED driver.
9. should have medical standard.
For white balancing, we need each channel control through programming
Beat Regards,
Tom Liu