This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A: Do you have data how much current TPS61021A can output at start-up?

Guru 29720 points
Part Number: TPS61021A

Hi Team,

I understand TPS61021A is recommended no load at start-up.

1)
Do you have data how much current TPS61021A can output at start-up?
I suppose Vin=0.9V and Vout=1.8V in this case.

2)
Is there any device that can output more than TPS61021A at start-up?
My customer's requirement is the following.
Vin: 0.9V
Vout: 1.8V
Iout (max): 1A

Best Regards,
Yaita