Part Number: TPS61032
Dear TI Team
I would like to ask about Output Capacitance(Cout).
When checking the TPS61032 data sheet, the minimum value of the output capacitor is stated as 22μF.
However, our customer is trying to set Cout=0.1μF.
(Because their designed board doesn't really care about the magnitude of the output voltage ripple)
If the capacitance of the output capacitor is set to 22μF or less, is there any problem other than the large output voltage ripple?
*Conditions are considered below.
Vin=2.8V
Vout=5V
Iout=0.52A
Best Regards,
Y.Ottey