Other Parts Discussed in Thread: LM3489
Hi
In Youhao Xi's article "Adjusting VOUT in USB Type-C™ and wireless charging applications, part 1" (link below),
there is an example presented to use switched resistor branches to program additional VOUT levels (Figure A)
However, due to the risk of triggering false OVP events when switching, another design is proposed, utilizing a FET and an RC-net (Figure B)
So, my question is, instead of incorporating three extra FET's and three extra RC nets, wouldn't it be possible to add a Capacitor like in Figure C? If not, why not? If so, how is a suitable value calculated?
And thus being able to use open drain outputs on an MCU to sink the resistor required for the wanted VOUT to GND.
Thanks, Thomas
Figure A:
Figure B: