This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: The problem with TPS63070

Part Number: TPS63070


When I was testing TPS63070, the input voltage was 4.6V~5.2V. When starting with load, the voltage could not output 5V. It can output 5V2A when the load is connected after it is started. Why does this problem occur? Does the TPS63070 fail to start under heavy load? If so, what is the recommended chip? I want 4.5~5.2V to 5V@2A.

(Use electronic load and electronic power supply during testing)