Could you provide a method for automatic load removal,for bq7791500 4 cell mode.
must to use over voltage, under voltage, cell balancing,and temperature protection. No other devices found.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you provide a method for automatic load removal,for bq7791500 4 cell mode.
must to use over voltage, under voltage, cell balancing,and temperature protection. No other devices found.
Hi,
Almost all of our BQ77915xx devices require load removal to recover from certain faults. This is detected by measuring the voltage on the LD pin. If the voltage on the LD pin is less than VLDT (approximately 1.3V), then the device will recognize that the load has been removed. If VLD is greater than VLDT, the device will recognize that there is a load present.