Hi,
I would like to check with you if TPS7B8250-Q1 in SSOP package will be able to dissipate some pulses of load current.
Load profile here is to supply an RF module which consume around 300mA during 100us every 1ms.
The ambient temperature is Ta= 105°C
Vin = 16V
Vout=5V
Iout = 300mA
Duration = 100us
Période = 1ms
Rest of the time, the module RF is turned off, where Iout of the LDO is below 10mA.
Can you please confirm if this is ok for TPS7B8250-Q1?
Thanks!,
Mohamed