This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73605EVM-5V-2MHZ: LM73605 EVM circuit is not able to deliver the rated current of 5A at 5V

Part Number: LM73605EVM-5V-2MHZ

Hello,

Based on this EVM and using the same schematic, I have designed a board. But the max current rating available without voltage fold back is only 3A. Of course,the layout is not exactly same but the circuit is. Any tips on where I could have gone wrong.

Thanks.