This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825B-SP: UC1825B-SP - Duty cycle control through external methods

Part Number: UC1825B-SP
Other Parts Discussed in Thread: UC1843B-SP,

Hello,

I am considering the UC1843B-SP for a non-synchronous buck application. The issue I am having trouble resolving is direct duty cycle control through external means. I have found an application note that describes methods of "voltage mode control"; however, I am trying to identify a method to use an external DAC for example. The goal is to input a voltage range into the control loop to directly impact the output voltage. If there are examples or application notes detailing this, that would be helpful.

Thank you