Other Parts Discussed in Thread: TPS25833-Q1
Hi
The customer applies TPS25840-Q1 to the cluster project.
We need answers to the customer's questions.
Customer enquiries:
1. The current requirement specification is USB A-type connector specification.
In this case, what is the maximum current support?
2. Should I connect the TPS25840-Q1 directly to the USB 3.0 AP port and configure the Vbus line as tps25840?
In this case, will it be possible to support up to 3.5A fast charging depending on the battery condition of many devices (iPhone x, Samsung)?
3. USB BC1.2 can charge up to 1.5A, but 2A or more when configured with TPS25840. Is that right?