This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to generate the 1.2V rail ( up to 200mA) from 1.8V supply and when looking at this device it states input voltage should not be less than 2V. I also looked at new series TPS7A20 however I need part already in production. My operating temperature is -55 to +125 deg C ambient. What do you recommend that will provide some margin on dropout voltage as well?
Thank you,
HSG
Hello,
Check out the TPS73101-EP.
You can also check out the TPS784. It has actually been tested down to -55C, as can be seen in the TC plots.
Best regards,
Nick