Hi team,
I am designing MCU reset circuit using TPS3840-Q1 as below.
VDD = button battery <4.5V
Vthreshold = 2.2V
V pullup = 1.8V
Pull up register value = 10kohm
Output I/F = Active Low Open Drain
1. Could you advise the VOL curve under the condition above just like Figure19, 20 in the datasheet?
2. How much will the output leakage current be?
3. How much is the minimum reset time delay (tD) at CT pin = Open?
regards,