Other Parts Discussed in Thread: LM5022, LM5156
Tool/software: WEBENCH® Design Tools
Hi Team,
The customer tried to simulate LM5002 in Webench in Boost topology with the specification below but he received an error message: Design cannot be created!
The error occurred at different Vout and Vin Max. It seems the error appears when the difference between Vout and Vin Max is 27V and above.
Vin Min = 9V
Vin Max = 50V
Vout = 50V
Iout=0.5A
Regards,
Danilo