Dear Sir,
Do you have the LED Driver Calculator Tool of TPS92641 ?
We Design the PWM Dimming for LED Driver
VCC Input 48V
Output 29.12V / 10.36A
KIng Lam CSAL-HKG
King.lam.kl.choi@edal.com.hk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
Do you have the LED Driver Calculator Tool of TPS92641 ?
We Design the PWM Dimming for LED Driver
VCC Input 48V
Output 29.12V / 10.36A
KIng Lam CSAL-HKG
King.lam.kl.choi@edal.com.hk
Hi,
Sorry, we don't provide the calculation tool. BTW, what parameters do you want to calculate?
BR,
Robin
Dear Robin, Thanks for your quick reply!!
In the Circuits Design for VCC= 48V
Output for LED for +29.12V / 10.36A
How to Cal. Resistor value of the IADJ, RON and CS use Resistor to match the Circuits .
Lam CSAL-HKG 2331002610
Hi,
RON is used to set the switching frequency, please refer to section 8.2.1.2.3 and 8.2.2.2.3 of datasheet.
IADJ is used to set the current sense voltage, please refer to section 8.2.1.2.3 and 8.2.2.2.4 of datasheet.
CS is the current sense pin and once you have set the current sense voltage, you can calculate the Rcs= current sense voltage/10.36A. Rf can be set 1kOhm.
BR,
Robin