This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12V Lead Acid Battery Charger IC

Other Parts Discussed in Thread: BQ24610, BQ24725A

Hi,

I need to design a 12V lead acid battery charger with the capable to change with the current of 3A.

As the main supply from a AC to DC is only 13.8V, I believe we will need to add a boost converter to allow the charger to be charged to 15.6V (or 14.4V?).

Efficiency is critical as the charger is required to meet the California Energy Commission (CEC) Battery Charger system or the BC mark.

Thanks,

San Lee