This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568: higher input voltage version

Part Number: TLV62568

Hi,

my customer is using TLV62568 to convert 5V USB input to 3.3V.

But they will do surge test on the USB port, and the TVS diode they use will only clamp the input voltage to 7V, which exceeds the maximum voltage rating of TLV62568.

Then we would like to know if we have pin to pin part with TLV62568 but higher input voltage range, thanks.