This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: UCC2897A VS LM5026

Part Number: UCC2897A
Other Parts Discussed in Thread: LM5026

Hi Support team 

may i have comparison table between UCC2897A VS LM5026 

  • Hi Red Yen! 

    Thanks so much for getting in touch and for your interest in these devices! Other than the features highlighted here, they are very similar devices. Please see the table below: 

    Features UCC2897A LM5026
    High Voltage Start Up 110V 100V
    FET Drive Capability +/- 2A +/- 3A
    Active Clamp FET Compatibility Only P-FET Both P-FET and N-FET
    Line Over Voltage Protection Yes No
    Max Duty Cycle 70% 80%
    Thermal Shutdown No Yes

    Thanks again for reaching out, I hope this information helps! 

    Aidan Davidson