Hi,
I intend to use TPSM82821 in my new design, and I have some questions regarding the product:
1- The product status is ‘preview’, is there any release date?
2- Will it be Ok to use this product to power FPGA (1.2V and 3.3V)?
3- I need to power a transceiver which consume about 0.8A, via a transformer, in transmit mode, and around 50mA when going into receive mode and vise versa. The transceiver uses a 47uF capacitor. Can I use this product with those requirement?
Since my product is very small (about 3cmm X 3cm), I need the smallest DC/DC with minimum additional components, is there any other DC/DC that can be used with those requirements?
Generally I am using LMZ10501silt for my designs to power FPGAs, but this product seems to requires more capacitors and it's a consume more space. will it be OK to power the above transceiver with LMZ10501silt, if the TPSM82821 release is not set yet?
Thanks!
Yossy Goldenberg