Good morning.
I'm evaluating the EPC9055 GaN module which using LM5113 as a gate driver for GaN MOSFETs.
First of all, my final goal is to operate the circuit below.
But it won't work. Power didn't flow to the output.
After I check the waveform, the EPC9055 output is not working properly. it isn't a square wave.
So I detached the full-wave rectifier part, re-checked the output of the EPC9055 like the circuit below.
Note that the Capacitor and Inductor in the output side circuit of EPC9055 works in the Resonance point.
The Center-bottom resistor is the PCB path resistor and the right side of the resistor is the load resistor which is several ohm(<10ohm).
With this condition, also didn't work properly.
After I check the gate driver in EPC9055, they use LM5113 as a gate driver and they are bootstrap type, Half-bridge driver.
To drive bootstrap type driver, the drain-source of the bottom switch should be connected with the load as the figure below.
I tried to add 10ohm as the load resistor, run the EPC5099 at the 1 Mhz PWM frequency.
it worked properly I guessed as the figure below.
So the question is,
1. If it is the path to charge the bootstrap capacitor is like the figure below,
What is the difference between using the only resistor as the load resistor and the RLC circuit as the load at the resonance frequency?
because the typical LLC converter uses the half-bridge as the input.
2. If it isn't working at my circuit, what should I add a component to charge the bootstrap capacitor?
Thank you for your help.