Hello,
I can see from the block diagram in the datasheet that the device has a SMBus 1.1 interface (system management bus) but I cannot find in either the datasheet or the Technical Reference Manual if the device supports packet error checking.
I downloaded the SMBus 1.1 standard:
and it says "Version 1.1 of SMBus introduces a Packet Error Checking mechanism to improve reliability and communication robustness. Implementation of Packet Error Checking by SMBus devices is optional." Does this device support packet error checking?
Thanks!
John