Hi,
I have a question with regards to UCC25630-1EVM-291, I can't seem to understand the exact function of D10 and R21 components on schematic. Will product team be able to advise on this?
Regards,
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question with regards to UCC25630-1EVM-291, I can't seem to understand the exact function of D10 and R21 components on schematic. Will product team be able to advise on this?
Regards,
Leo
Hi Leo,
D10 and R21 are to help avoid opto-coupler saturation which causes a delay in the opto-coupler response and results in a delay in the transient response. Normally the FB pin voltage is loosely regulated to ~5.5V and the device will measure the amount of current that is pulled out of the FB pin as the feedback signal. If the opto-coupler starts to saturate and the voltage on the FB pin begins to drop, D10 turns on and sources additional current to the FB pin to try to prevent the opto from fully saturating. R21 sets how much additional current is sourced to the opto-coupler while D10 is conducting.
Best Regards,
Ben Lough