This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3890: As input is pulled low more than 10s, the output can have a short low pulse.

Part Number: TPS3890
Other Parts Discussed in Thread: TPS3820

Team,

Could TPS3890 meet our requirements as below image? (

. As input is pulled low more than 10s, the output can have a short low pulse. The short pulse is used to disable another IC.

)

Roy