Other Parts Discussed in Thread: LM258
Hi
Can someone please help resolve the simulation problems with my customer's TINA circuit attached? I did try to run a transient simulation and I get an error message with issues with a few nodes.
Here are the circuit goals and some issues from the customer:
The transfer ratio of the current sense is 100; the voltage ratio of the transformer is 8/3; and the frequency of the PWM generator is supposed to be 300KHz, but I was not able to set that because when I open the voltage generator VG1, there is no field to set the frequency. The input voltage is 28V and the output voltage is supposed to be 28V. I plan to do the transient and the AC analysis. Please, could you help me in troubleshooting the design?
One more thing I would like to draw your attention to is the ground at the secondary of the transformer. It should be different from the ground at the primary, but I was not able to find another ground symbol to do that.
Thanks for your help!
Best regards,
Jim B
/cfs-file/__key/communityserver-discussions-components-files/196/LM5041-Simulation-Issue.TSC