Other Parts Discussed in Thread: TPS92641
Hello,
We have the development board with added Q3 for external Shunt FET PWM Dimming.
R1 is decreased to 15 kOhm to get a switching frequency of about 1 MHz.
Vin = 48 V
With an LED string with Vo = 29 V everything is good. The current is regulated to 1 A.
yellow: PWM input magenta: LED current 1 A
With an LED string with Vo = 33 V the current breaks down to less then 0.5 A.
Is there a minimum difference or a minimum factor between input voltage and the LED voltage?
Or is something in the dimensining of the evaluation board not suitable for our application?
We would like to use LED voltages up to 42 V with an input voltage of 48 V.
Thank you.
Best regards
Werner