Input PMW Duty clcye 0% to 95% can operate normally?
As shown in the figure below:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[quote user="user4772772"]
Part Number: CSD95379Q3M
Input PWM Duty clcye 0% to 95% can operate normally?
As shown in the figure below:
Hi,
The recommended PWM on time duty cycle is to be less than 85%. While the minimum PWM on pulse is 40ns, so the minimum duty is depending on your switching frequency.
Best,
Qingquan
Thank you for reply!
I will ask a question:
UCD7242 PWM input duty cycle can be from 0% to 95% frequency 500KHz?
Hi,
I am not familiar with UCD7242, please create another post to get help from UCD support team. Thanks!
Best,
Qingquan