Hi,
We are using TPL7407 in order to drive 6 solenoid valves which have 24V operating voltage and approximately 250 mA current rating per valve. The valve driver circuit has been designed as advised in its datasheet, I added reverse schottky diode to OUT7 (which is actually unused) and Ccom capacitance with 100V voltage rating. All digital inputs are coming via optocouplers to preserve microcontroller side, and there is a resettable fuse, 1000 mA trip current, to avoid excessive current usage on COM power line. Our problem is that it sometimes breaks suddenly, you can see its photo below. I am being suspicious of loose contact between solenoid valves and the circuit, and it creates sudden current peaks but I guess it should be handled in solenoid driver IC. Do you have any suggestions about it?