This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE4275-Q1: TLE4275-Q1 reset out maximum delay query

Part Number: TLE4275-Q1

Dear TI Team,

We are using TLE4275-Q1 and the query is regarding Reset out (Pin 2) of LDO.

As per the datasheet, reset delay can be vary depending on Cap value. which is around 15.4mSec by using 47nF cap.

Also, as per the formula given in the datasheet, the delay value coming 15mSec with 47nF.

Now Query is that we have a special requirement of around 70mSec delay, which is looking achievable with 220nF as per calculation with the formula given in the datasheet.

Can you please confirm that if we use 220nF or bigger Cap value then is 70mSec delay practically achievable or any limit?

and what is the maximum delay we can achieve by increasing the value of cap more and more?

Regards,

Sachin Garg

Hardware designer

Assistant Manager

Marelli India Pvt. Ltd