Other Parts Discussed in Thread: UCC28180,
Hi Team,
I am working with a customer who is using UCC28180 in an upcoming power supply design and they are validating the solution using UCC28180EVM-573.
- What are the changes that were made in updating the design from Rev A to Rev B?
- In this documentation there are several frequencies used to show how the choice of inductance can improve Harmonic Distortion and the choice of ripple current can also affect this. Frequencies as low as 18 kHz with large inductance used – are there any issues going to higher frequencies (higher than the 120 kHz example)?
- There are some phase/gain plots (Section 6.9), can you verify what switching frequency was used for this example?
- Is this crossover freq suggested regardless of switching frequency (given the 50 Hz input power)
Thank you!
Garret