For Writing FC1 and FC2, as per datasheet and FC1 and FC2 Issues in forum stated that generate the LAT signal along with SCLK signal.
My Question is:
For SPI Clocks (SCLK) through SPI data writing in SPI mode, how we can write the LAT signal in parallel with SCLK. It is possible only by keeping SCLK as GPIO and Manual Generation of SCLK without using SPI module. It Works for Single Driver Usage.
But my application demands more TLC59581 to be daisy chained, Then how can we generate SCLK and LAT signals at a time in all daisy chained Drivers. This is applicable for GSdata Write also.
Is it ok if i push all the required Data(FC1/FC2/GSDATA) in all required Daisy chained Drivers and then separately generate the SCLK pulses with Don't Care Data by keeping LAT signal required state?
I am eagerly waiting for your reply.