Other Parts Discussed in Thread: TPS61023
Hello team,
Customer test TPS61023 with our EVM in the below condition
<Conditions>
Vin : 2.7V
Vout : 3.293V
R3 = 680kohm, R4 = 150k ohm (in the EVM)
<Test results>
- Vout : 3.41V Iout = 0mA
- Vout : 3.38V Iout = 100mA
- Vout : 3.36V Iout = 200mA
- Vout : 3.32V Iout = 300mA
- Vout : 3.31V Iout = 400mA
- Vout : 3.32V Iout = 500mA
As the above, in the current more than 300mA, the output voltage is stable but there is large variation of Vout at less than 200mA.
I think that one of the reason is that TPS61023 would enter PWM mode but I would like to know the reason why there is large variation.
And also could you advise the threshold to enter PFM mode ?
Thank you and best regards,
Michiaki