Other Parts Discussed in Thread: LMG1210
Hi ,
As the EPC2001 GaN FET is able to source 25 A .
What are the changes required to do in this EVM to get 25A current out.
With Regards,
Ganesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
As the EPC2001 GaN FET is able to source 25 A .
What are the changes required to do in this EVM to get 25A current out.
With Regards,
Ganesh
Hi Ganesh,
Due to thermal limitation, the EVM is limited to 100V, 10A max current.
For operation above 10A, you will considerations thermal management techniques including additional heat sinks, forced air, and significantly reducing the switching frequency to limit the power dissipation.
You will also need to update the inductor and other components as L1 on the board is 4.7uH, 10.5-A inductor.
Regards,
-Mamadou
Dear Mamado,
Thanks for your reply. I want to use this solution for Core supply of Zynq MPSoC. its 0.75VDC/23 A.
I want to use the buck above 10MHz switching . can you suggest me some solution.
With regards,
Ganesh Singh
GaN solution should be better as it fits all other needs. Apart from it can you connect me to any APP engineer which is expert in GaN design so i can forward him my Power tree.
With Regards,
Ganesh Singh
Ganesh,
I can help address any specific applications support related to the gate drivers in your application.
The GaN power stage team might be suited to address your specific needs in which case you will post on a separate thread with the specific part number of interest from the GaN team.
While you create a separate thread, I will go ahead and mark this thread as "resolved".
Feel free to post any additional questions on the LMG1210 on this thread.
Regards,
-Mamadou