Hello;
There seems to be indeterminant behavior when the TLV71333's output is pulled to another 3.3V rail, while its input slowly rises from ground, and EN is tied to Vin. During a transition from a buck switcher (which supplies the 713's input) from another 3.3V LDO, on some boards it appears that the 713's active pull-down gets enabled, when its input is below its minimum, even though EN is tied to Vin
I note from the datasheet the graph of the power up and down sequences, where the 713 doesn't begin operating until Vin is approx 1.3V. I understand this scenario is out of bounds, but can you clarify what short of behavior to expect when its Vout is pulled to 3.3V, while its input is much lower? My assumption is that, once it begins to regulate, it will just turn of its pfet, but since its body diode will conduct, will that somehow enable the active pulldown??
Thanks