This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940EVM: Can we replace the onboard FET: AOB290L with CSD19536KTT?

Part Number: BQ76940EVM


Hello,

My application requires a continuous discharge current of 30A, which can be easily done by CSD19536KTT

I also noticed that the same FET is being used in TIDA 00792.

Both have nearly the same Vgth and Rds of CSD19536KTT is comparatively smaller.

So, can we desolder Q2 and Q4 i.e. AOB290L, and replace them with CSD19536KTT to achieve max charge/discharge current of 30A?

Thanks,

Nishil