This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD88537ND: NexFET Structure

Part Number: CSD88537ND

Dear PIC,

Our customer ask us the NexFET Structure and could you tell me the following questions.

If the MOS-FET has an element under the bonding pad, is there any evidence below that supports the strength and reliability of the interlayer insulating film structure against bonding stress?

-The aluminum layer of the bonding pad is formed sufficiently thick (reference 3um).
-A barrier metal is provided under the bonding pad to reduce bonding stress (example: TiN / Ti).
-It has been confirmed that cracks do not occur in the interlayer film even under the worst conditions of wire bonding stress (ultrasonic power, load, temperature, etc.).
-Reliability evaluation is performed that can detect intermittent defects such as load fluctuation monitors.

Best Regards,