Hi Team
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
Hi Yuichi,
A few comments:
For output accuracy (4-1), the TPS7A52 accuracy spec already includes the line and load regulation since the spec is across the entire range for Vin and Vout. So you just need to add your resistor divider error to get the total accuracy.
For dropout (4-2), the minimum headroom that the application will have will be Vin(min)-Vout(max)=3.6*0.9817-3.3*1.0075=209.4mV (which is more than the max dropout of 170mV listed in the PDS which is good).
For Tj (4-3), the max drop across the LDO is the 409mV you calculated, and the Tj you caluclated is correct based on the JEDEC standard board. You can likely get better with a real PCB layout but at the current 84C you are at a reasonable max temperature since this device is specified up to 125C.
The schematic doesn't show the schematic for the TPS7A52, so I wasn't able to review the schematic to check min/max Cin, Cout and the resistor divider values. If that is needed please follow up.
Hi Kyle
Hi Kyle
Hi Yuichi,
I don't see any problems with the schematic, though I have think it would be good to evaluate the inrush current just to make sure your system doesn't have any startup concerns due to the amount of output capacitance.
Hi Yuichi,
Whether you use Bias or not will not have any effect on the thermal dissipation of the LDO. Almost all of the thermal dissipation occurs due to the current flowing from Vin to Vout (though the resistance of the pass device). At full load the power dissipation due to the ground current is only bout 3-4% of the total power dissipation.
I don't think the LDO itself could heat the ambient air enough to cause a significant increase in the ambient temperature. If you have 2A flowing through the LDO and only 300mV from Vin to Vout, you're only talking about a power dissipation of 0.6W. The downstream loads would be consuming 2A at 3.3V which is 6.6W and their thermal dissipation should dominate the heating of the ambient air compared to LDO.
Assuming you have an enclosure around your system, you'd need to do a thermal simulation of your whole system to determine the ambient temperature when the system is running.
Hi Kyle
Regards,
Yuichi
Hi Yuichi,
Sorry for the confusion, I was evaluation the schematic looking at the automotive version of the TPS7A52. I've amended my removing the question about GND and NC pins.
As for the thermals,I better understand your request about Figure 39 and of the LDO heating up the capacitors. As you mentioned the EVM shows that the heating isn't very much but below I've overlaid them so you can get a sense of where the capacitors are in the heat map. The PCB around the input and output caps are likely ~45C, while the PCB around the Bias cap is likely ~49C (though as you mentioned you are not using this capacitor). The other components will be significantly cooler.
Hi Kyle
Thank you for your kind reply. I was relieved at the temperature. Check the inrush current for the entire power supply system. Currently, it is in the unit design stage, so we will proceed with the circuit presented.
Are there any other issues?
Regards,
Yuichi
Hi Kyle,
Regards,
Yuichi