This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3414HVMREVAL: Issue on PWM dimming frequency

Part Number: LM3414HVMREVAL
Other Parts Discussed in Thread: LM3414HV, LM3414

Hello everyone, I bought the LM3414HVREVAL board to test the LM3414HV chip because I want to use it for a project of LED driver. I found some issue with the PWM dimming frequency that confused me, please can you help me?

The issue is: 

- With a PWM frequency from 200Hz to 400Hz at 70to80% of duty cycle the LED flicker a lot and this is unacceptable;

- With a PWM frequency higher that 1kHz instead the LED works great and no problem found when dimmered.

So I don't know how this can happen, on the datasheet of the component LM2414HV there is: 

" To ensure normal operation of the LM3414/HV, TI recommends setting the dimming frequency not higher than 1/10 of the switching frequency..."

And this is exactly what I've done. Could you please help me with this issue?

I want a PWM frequency from 200Hz to 400Hz because most of commercial dimmer work at this output frequency.

  • Hi Pacini1,

         Could you share some test waveform about the Inductor current, Vout and output current? And how about your supply voltage and LED configuration?

    BR

    Sean

  • Hello Mr. Sean,

    unfortunately I can't share with you this information. I don't have any instrumentation to test that, I have only a multimeter with me. The circuit is exactly the same as the LM341HVMREVAL evaluation board.

    There is a way to solve the problem without the information you asked for? 

    Thank you, 

    Claudio Pacini.

  • Hi Pacini,

        I'm sorry that give out more analysis since there are no test waveforms. Maybe you need to check your configuration and PWM signal again.

    BR

    Sean