Hi there,
We are using TPS7A49 LDO to convert 15 V DC to 5 V DC (Current Requirement: 20 mA). Our 15V DC source can supply maximum current of 200 mA. Please let us know that if the ADJ pin of LDO gets short-circuited to GND in case of any fault, then what will happen to the LDO output voltage? Will it become equal to the LDO input voltage? What would be the impact on load current flowing through the LDO?
Thanks and Regards,
Surya Mohan